{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
ION7400 series front display simulator
Issue
Functionality of the ION7400 series meter may need to be implemented when instructing a customer through a setup procedure using an ION7400 series meter.

Product Line
ION7400

Environment
ION7400 front display

Cause
Physical meter might be unavailable

Resolution
Download and install the simulator
Offline Meters, or meter simulators, are used on your Windows PC to emulate the meter hardware platform for the development and testing of meter application logic (a.k.a ION frameworks) using either ION Setup software or ION Enterprise Designer. Once the meter simulator is running, it can be accessed at the domain name "localhost" (127.0.0.1) with software on the same computer.


Schneider Electric Global

Attachment(s)
ION7400_Simulator_V001.003.001_Release.zip [1.85 MB]