Does the HMIG3U need a powered USB hub to power the XVGU and HMIZRA1?
Published date:
05 April 2019
Issue:
Does the HMIG3U need a powered USB hub to power the XVGU and HMIZRA1?
Product Line:
Magelis HMIG3U
Resolution:
No, the HMIG3U does not need a powered USB hub to power the XVGU and HMIZRA1. Each of the USB ports of the HMIG3U can supply upto 500ma of current. The two devices require 400ma each.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.