Browse FAQs

How do we decode the Date of Manufacture (DOM) on the Magelis series of HMIs?

Published date: 25 October 2019

Issue:
Where on the label of the Magelis HMI can we find information regarding the date in which the unit was produced? 

Product Line:
Magelis series of HMI, XBTG, XBTGT, HMIGTO, HMISTO, HMISTU, HMIGTU, HMIGK

Resolution:
On the back of a Magelis HMI, there is a sticker/label with the Date of Manufacture (DOM) on it. The code is typically 4 digits like this: 1533. For this particular example, it decodes as Year:2015, Week 33.

Therefore in general terms the date code is: YYWW where YY is the last two digits of the year and WW is the week number in that particular year.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.