undefined undefined
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to show a record for each alarm state change in Vijeo Designer?
Issue:
Looking for a way for the HMI to record a separate entry in the Alarm Summary whenever the alarm transitions from Active, ACK'd, and return to normal.

Product Line:
Vijeo Designer (all versions)

Resolution:
In Vijeo Designer, it is possible to show a separate record in the Alarm Summary for each state change of an Alarm Variable. To do so, simply set the property "Alarm & Events List" to Log.

By default, this property is set to "Active". In this mode, the Alarm Summary will only show alarms that are still Active. When the states change from Active to RTN, the record disappears.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: