Maximum number of Sercos axis that the LMC078 can support
Published date:
06 May 2019
Issue: Maximum number of Sercos axis that the LMC078 can support
Product Line: LMC078
Resolution:
With the new hardware reference version RS02 (HW Code 0224013000000000) the number of supported axis by the LMC078 controller is now 24 axis (compared to 12 axis) in 4 ms.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.