{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Does the SR2MOD03 wireless modem support 3G networks?

Issue:
Does the SR2MOD03 wireless modem work with 3G networks?

Product Line:
SR2MOD03

Resolution:
The modems with manufacturing dates greater than or equal to 1630 support 3G and are six Bands (Band I (2100 MHz), Band II (1900 MHz), Band IV (1700 MHz), Band V (850 MHz), Band VI (800 MHz) and Band VIII (900 MHz)) in 3G UMTS/HSDPA/HSUPA.

Did this answer your question?

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.