{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
The user manual does not describe the response from the BMXNOR0200 if an unsolicited event occurs in Class 1 when the Class 1, 2 and 3 unsolicited option is enabled.
Issue
Describe what is the response from the BMXNOR0200 if an unsolicited event occurs in Class 1 with Class 1, 2 and 3
when the Class 1, 2 and 3 unsolicited option is enabled.

Product Line
BMXNOR0200

Environment
Windows 10

Causes and Fixes
The user manual does not describe the response from the BMXNOR0200 if an unsolicited event occurs in Class 1
when the Class 1, 2 and 3 unsolicited option is enabled.

If the BMXNOR0200 is configured for a 'DNP3 Unsolicited Report by Exception' by defining the Event Class 1,2,3 with
Unsolicited enabled, an unsolicited Class 1 event occurrence will cause the following  '
Unsolicited Report by Exception behavior':
  • The module will report all events from any class that has the unsolicited option enabled.


Schneider Electric Global