Browse FAQs

Logipam SFT2885 V3.3 Download

Published date: 31 October 2019

Issue
Logipam (SFT2885) is a standalone software used for programming dedicated functions on SEPAM Series 80 relays

Product line
SFT2885, SEPAM 80

Resolution 
To download the latest version of the software, V3.3, download the attachment.
For more information about logipam, please refer to the logipam manual found below.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.