{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the smallest motor you can run on the ATV630 and ATV930 Process drives?

Article available in these languages: Spanish

Issue:
What is the rating for the smallest motor you can use on an Altivar Process Drive

Product Line:
ATV630 and ATV930

Environment:
All

Cause:
Wants to run a smaller motor on the larger drive.

Resolution:
The nominal motor current can be set to 25% of the drives current rating and the motor thermal can be set to 20% of the drives current ratings.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Global