Browse FAQs

What are the PC Hardware Requirements for SoMachine v4.2?

Published date: 04 September 2018

The PC Hardware Requirements for SoMachine v4.2 are:

Processor:
MINIMUM: Intel® Core™ 2 Duo* or equivalent
RECOMMENDED: Intel® Core™ i7 or equivalent

RAM
MINIMUM: 3 GB
RECOMMENDED: 8 GB

Free Hard Disk Space
MINIMUM: 8 GB including the memory space for the typical software installation, temporary space for execution and space for saving applications
RECOMMENDED: 15 GB for the full software installation, temporary space for execution and space for saving applications

Drive
DVD reader

Display
MINIMUM: Resolution: 1280 x 1024 pixel
RECOMMENDED: Resolution: 1680 x 1050 pixel

Peripherals
A mouse or compatible pointing device

Web Access
Web registration requires internet access system

Virtual Machine usage
· When using a VM running SoMachine V4.2, be sure to fulfill the minimal requirements especially for RAM, hard disk space and number of Cores inside the VM. Otherwise unexpected errors may occur (e.g. out of memory exception when installing SoMachine V4.2).




 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.