{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to size the non-uniform busways in the EcoStruxure Power Design - Ecodial?
While connecting and sizing the non uniform busways follow the below steps in EcoStruxure Power Design - Ecodial

1. A rising busway has to be selected from the symbol pallet.



2. The busway can be calculated for uniform or non-uniform tap off unit’s distribution.



3. Set length of the non-uniform busway



4. When the busway is set to non-uniform distribution, the distance from origin must be set for each tap-off unit.



5. After calculation, for non-uniform busway, the short circuit currents and voltage drops are calculated for each feeder.



6. If the distance from origin of a feeder is more than the length of the BTS, after the calculation in the alarm window error will appear.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.