{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
After conversion of my SoMachine V3.1 project including an M258 to v4.2, TM5 modules configuration tabs are wrong
After conversion of a SoMachine V3.1 project including an M258 to SoMachine V4.2, TM5 modules configuration tabs are wrong.
For example with DI12DE :
Normally it should be like this :



But this is what conversion gives:

Wrong "Outputs" folder is there.

Furthermore integrated TM5 modules data is not exchanged when converted project is downloaded to a controller.

It happens when conversion from V3.1 to V4.2 is not executed “directly” :
When V3.1 project is opened in SoMachine v4.2, a pop-up asks for project conversion. “Yes” should be answered right now.

If conversion is done later using “right click -> update device” then trouble with TM5 modules happen.

This will be corrected in SoMachine V5.

Schneider Electric Global