undefined [object Object]
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
IEC or EN60204-1 compatibility for ATV600/630?
IEC 60204-1: is standard for Safety of machinery - Electrical equipment of machines – Part 1: General requirements. This gives the stop category of safety function.

On ATV630 there is STO function This safety function corresponds to an uncontrolled stop in accordance with stop category 0 of IEC 60204-1.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: