Is there a blank NetShelter door badge available? If so, what size is available and how many are in the package? Can APC provide custom door badges?
Published date:
05 July 2019
Issue:
Customers may want to have their logo on the cabinet.
Product Line:
NetShelter SX
Environment:
All models, all serial numbers.
Cause:
Customers may not want the APC by Schneider Electric logo on their cabinets, or may want additional badges.
Resolution:
We offer sku AR7001X384, which is a pack of 40 blank door badges, The door badge is oval, and the dimensions are 71.5 mm wide x 39.4 mm high.
To date we have not offered custom printed door badges attached to the cabinet. To process a request please contact your APC Sales Rep, or the CustomRacks team.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.