Browse FAQs

Error "Number of variables exceeds the maximum allowed. [500]" appears when building Vijeo Designer application

Published date: 28 October 2019

Issue:
Unable to build Vijeo Designer application. The compiler stops and displays an error regarding the number of variables with "Log Users Operations on Variable" being more than 500.

Product Line:
Vijeo Designer (all versions)

Resolution:
This error occurs when you build an application that has more than 500 variables with the property "Log User Operations on Variable" enabled. To resolve this issue, please limit the application to use 500 or less variables with this property enabled. This limitation has been put in place to limit the DRAM usage of the Event Logging feature.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.