{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What are the mechanical characteristics of Pm2225 meter ?
Following are the Mechanical characteristics of PM2225 meter :

IP degree of protection (IEC 60529-1) Front display: IP52
Meter body: IP30
Panel thickness maximum 6.0 mm (0.25 in) maximum
Mounting position Vertical
Display type LCD display: Monochrome graphical LCD
Keypad 4 button with intuitive navigation
Front panel LED indicators Green LED (heartbeat / serial communications activity)
Amber LED (alarm / energy pulse output)
Weight ~ 300 gms
Dimensions W x H x D 96 x 96 x 73 mm max
Protection features Password protected for set-up parameters

Schneider Electric Global