{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
ATS46 soft starter is blowing control power fuses on power up.
Issue:
Blowing control power fuses on ATS46 power up.

Product Line:
ATS46

Environment:
All

Cause:
NA

Resolution:
The soft starter is obsolete and repair parts are limited or obsolete.

There could be an issue with the transformer and/or cooling fan in the soft starter.

Suggested sending the soft starter in to the repair depot or replace the ATS46 with the the ATS48 soft starter.

Schneider Electric Global