{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the output current of an EVH2S22P04K EvLink Wall box charging station be permanently limited? If so, to what level?
EVH2S22P04K can permanently limit its output current/power.

To limit the power:
1. activate power limitation mode in the charging station setting (see page 1 of Attachment1)
2. connect input E6 to 230V (see page 2 of Attachment1). The maximum charging power is limited as long as on the E6 is 230V.

The EVH2S22P04K is 32A station, therefore the power can be limited to level 16A (see page 2 of Attachment1).

Schneider Electric Global

Attachment(s)
Attachment1.pdf [252.18 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: