{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can we have different DNP sever sessions to talk with different SCADA clients
Question:
Can we have different DNP sever sessions to talk with different SCADA clients. Cause customer has two SCADA clients & they have respective master/slave address.


Answer:
No.
DNP3 as TCP server only supports one session with one set of master/slave address.
So customer has to adjust the two clients as same master/slave address to talk with the common session in NOR.
If they would like two customized sessions at NOR part, two NOR modules are needed.

Schneider Electric Global