{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do we evaluate number of modifications in M580 HSBY
Issue:
How do we evaluate number of modifications in M580 HSBY?
Would every variable change or section change  be taken account as 1 number of modifications.?

Product Line:
Modicon M580

Environment:
EcoStruxure Control Expert
Unity Pro

Resolution:
No.The number of modifications configured at Hot Standby tab of CPU is used to specify the maximum number of modifications allowed between Primary CPU & Standby CPU.
The number of modifications increase by 1 upon every build change (no matter how many variables or sections you had changed within the same time period)

Schneider Electric Global