{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why, while configuring an IO module via the Dual Setting (Configure > Protection), does Ecoreach change the parameters for Inputs 5 and 6 of the IO module? (Configure > IO Config)
Issue:  While configuring an IO module via the Dual Setting (Configure > Protection) through Ecoreach the parameters inputs 5 and 6 of IO module are also changed.

Product Line: IO module, Ecoreach.

Cause:  Every time that user changes the configuration of an IO module and Control Unit, Ecoreach modifies the Inputs 5 and 6 of the IO module to ensure maximum coherence and security.

Resolution: ​After configuring the Dual Setting, check that the Inputs 5 and 6 of the IO module are configured properly. If not, configure them as required and click Write to Device.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.