Browse FAQs

From where can the Multi-loader's firmware version V3.18 be downloaded?

Published date: 04 February 2019

Issue:
Unable to copy programs with ATV320 drive using Multi-loader device.

Product Line:
Multi-loader tool

Environment:
All models and serial numbers with firmware revision below 3.18

Cause:
Firmware update needed to communicate properly with newer drives.

Resolution:
The firmware to upgrade from 3.18 firmware can be found at the link below.  This will update a multi-loader that is currently at 3.08 firmware or above to 3.18.

https://www.se.com/ww/en/download/document/MLD_FW_from_V3.08/

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.