Browse FAQs

What is the UL Type 1 Conformity Kit for the ATV630 High HP drives?

Published date: 27 November 2018

Issue:
Customer is trying to select a UL Type 1 Conformity Kit from the ATV630 catalog.  The catalog lists two options.
VW3A9212
VW3A9213 (without brake resistor)

Product line:
Altivar 630, ATV630
ATV630C22N4
ATV630C25N4
ATV630C31N4

Environment:
models listed

Cause:
Catalog error

Resolution:
The ATV630 drive cannot use Brake resistors.  So the only available Type 1 Conformity kit is VW3A9213.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.