Resolution:
ILF fault is communication interruption between the option card and the drive. The first test will be to replace impacted option cards by known good cards to know if ILF fault follows the option card or the drive.
For example, swap impacted option cards with option cards where ATV320 drives are working fine.
If ILF fault is caused by option cards, replace them.
If you still have ILF fault despite the option card replacement, network overload may be the cause.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.