{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: Creating Write_Var Function for FC15 Write Multiple Coils in Unity
This procedure is prepared with Unity Pro v12 software and covers creating a FBD logic section for the M340 Write_Var function block performing a FC15 Write Multiple Coils operation from the BMXNOE0100 ethernet module to an ethernet server device which supports a Modbus FC15 operation.

Schneider Electric Global