Browse FAQs

What control circuit voltage is needed for the ATS48?

Published date: 10 January 2019

Issue:
What control circuit voltage is needed for the ATS48?

Product Line:
Altistart 48

Environment:
All

Cause:
Installation

Resolution:

For ATS48...Q the control circuit voltage is 220 - 15 % to 415 + 10 %, 50 / 60 Hz & ATS48..Y control circuit voltage is 110 - 15 % to 230 + 10 %, 50 / 60 Hz as indicated in the attached chart. This is AC voltage. 

Control voltage should be applied to the CL1 & CL2 terminals.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.