{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How can I use the two function buttons F1 and F2?
Issue
What is the purpose of the F buttons on the Easergy P3 relay?

Product Line
Easergy P3

Resolution
F buttons are freely configurable for various purpose, both buttons are connected to an activation LED. Typical use of (but not limited to) the buttons:
  • Control of an object
  • Change setting group
  • Activate/deactivate a function, e.g. auto recloser
  • Reset latches
  • Change or start/stop a programmable logic
Please check manual for configuration instructions.

Schneider Electric Global