Are the Open/Close control pushbuttons fixed to specific object?
No, Open/Close control pushbuttons can be defined to any of the 6 controllable objects by parameter “Object for control buttons” under Object menu. Same parameter can be found under Local panel conf menu.
Released for:Schneider Electric Global
Explore more
Range:
Easergy P3 Protection Relays
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.