Resolution:
SCF4 [IGBT short circuit] indicates that there may be a power component failure.
If the drive still faults on SCF4 with the motor disconnected and Output Phase Loss set to NO (CONF->FULL-> FLT-, OPL); contact the Drive Products Support Group at 888-778-2733, option 2 for Technical Support and then option 4 for AC drives and soft starts.
The following can also be done to test the drive by itself.
CONF, FULL, FLt (Fault menu) OPL (Output phase loss)= NO.
By setting above parameter, you can check drive without physical connection of motor.
Drive will follow frequency reference and control (Start/ Stop) command and will not trip on “Output phase loss”.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.