Browse FAQs

Is there a replacement for the TWDXCPRTC real-time clock cartridge?

Published date: 04 September 2018

There is no replacement for the TWDXCPRTC real-time clock cartridge.

- TWDXCPRTC is part of the Twido line of controllers which at this point is obsolete.
- The replacement for the Twido controllers are the M221 controllers. All M221 Logic Controller includes a Real Time Clock (RTC) system
- A customer looking for a TWDXCPRTC should be looking into converting his Twido project to a M221 / SoMachine Basic project. A Twidosuite project can be opened and converted easily into a SoMachine Basic project.
- Please contact the automation technical support at 888-266-8705 if you need to convert a Twido controller to a M221 controller

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.