{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why can't I see entries like FR1, CHCF, or CD1 in CoE in ATV320 VFDs with VW3A3601 EtherCAT comm card?
Issue:
Entries like FR1, CHCF, or CD1 in CoE in ATV320 VFDs with VW3A3601 EtherCAT comm card.

Product Line:
ATV320

Environment:
All

Cause:
Having access to these parameters through CoE allows easier configuration and also the potential for automated configuration.

Resolution:
Need V1.12 ESI file. It corrects the problem.

Schneider Electric Global