Is it possible in Unity pro to force %IW values directly from the Animation Table with M580?
Published date:
27 February 2019
Issue
Need to force analog input DDT in the M580.
Product line
M580, Unity pro
Resolution
It is possible now to force Analog inputs on M580 with unlocated data model (on Device DDT). it will not be implemented on located data, because Schneider focus is on unlocated Data with M580.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.