Browse FAQs

Is there a maximum number of writes to assign a Flash Memory PCMCIA TSXMFPP0002M?

Published date: 17 April 2020

Issue
Is there a maximum number of writes to assign a Flash Memory PCMCIA TSXMFPP002M?   

Product Line
TSX Micro, TSX Premium

Environment
TSXMFPP002M 

Resolution
The PCMCIA card TSXMFPP002M has a ST  Flash IC M29W160 and the average value of writes is 100,000 Program/Erase cycles per Block.
P.S.: Attached is the flash memory datasheet.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.