Browse FAQs

How can I add a Profibus GSD file to Unity Pro library of Generic DTMs?

Published date: 05 November 2019

Issue
How can I add a Profibus GSD file to Unity Pro library of Generic DTMs?    

Product Line
EcoStruxure Control Expert, M580, M340, Quantum 

Environment
BMEP581020, TCSEGPA23F14F, Unity Pro v13.0.

Resolution
The TCSEGPA23F14F (PRM) is a standalone module designed to provide Profibus DPV0 & DPV1 master capability to the M340, M580, Premium and Quantum ranges. Profibus slave configuration is based on GSD that is a data base file with the device information and I/O configuration that is provided by the vendor's. 
The PRM Master DTM and the PRM Gateway DTM includes an interface for converting any GSD file into a generic DTM in order to be integrated into the DTM catalog and used to configure a slave for the PRM.
  1. In the Unity Pro menu bar, select Tools -> DTM Browser
  2. In the DTM Browser, select the PRM_Master instance or PRM_Gateway instance as applicable
  3. Right click (DTM contextual menu) and select Device menu -> Add GSD in Library. The welcome page of the wizard opens.
  4. Click Next, select the location of the GSD File(s) and go forward until a page with finish option opens.
  5. Unity Pro hardware catalog has to be updated in order to use new devices with your Unity Pro project.
Update the DTM catalog of the FDT frame.
  1. Select in the Unity Pro menu bar Tool->Hardware Catalog
  2. Select DTM Catalog tab in the Hardware catalog windows
  3. Click the Update button for starting the update
​Now, EcoStruxure Control Expert has the device on its hardware catalog and it can be used with others Control Expert projects.

P.S.: You can download here the PROFIBUS Remote Master iso file.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.