What are the FDR parameters set to in the LTMCUF by default?
Published date:
28 November 2018
Issue:
Customer needs to know what the default configuration is for the FDR parameters in the LTMCUF HMI
Product Line:
Tesys T
Environment:
LTMCUF only. Does not apply to LTMCU
Cause:
NA
Resolution:
By default, when LTMCUF is new, the error F09 "No config valid" appears as the LTMCUF memory is empty. This is a reminder that a backup operation needs to be done before using the FDR services.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.