Browse FAQs

How do you wire and program an ATV630 to replace an ATV58 in a Trane Air Handler?

Published date: 20 November 2019

Issue:
Wondering how do you program an ATV630, to replace an ATV58, in a Trane Air Handler?

Product Line:
ATV630

Environment:
All

Cause:
Wiring and programming

Resolution:
A Trane Unit had a board that did the switching for the drive.  If you've wired exactly as before, you only need to Program [Complete settings] > [Command and Reference] > [Ref Freq.1Cfg]  to AI1 and [Complete Settings] [Input/Output] [R2 Configuration] to Drive Running.  Be sure to configure [Simply Start].

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.