Can the Altivar ATV340 programming be saved to the VW3A1111 Keypad?
Published date:
27 November 2018
Issue:
Can the Altivar ATV340 parameters be saved to the VW3A1111 Keypad?
Product Line:
Altivar 340
Environment:
All
Cause:
Configuration
Resolution:
The ATV340 works the same way as the ATV630 and ATV930. Browse to [Main Menu] > [File Management] > [Transfer Config File] > select "Copy from the drive" to backup to the keypad.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.