Browse FAQs

What is the difference between the B suffix version of the ATV312 Drive and the non B suffix version?

Published date: 07 February 2019

Issue:
What is the difference between the B suffix version of the ATV312 Drive and the non B suffix version?

Product Line:
ATV312.... B

Environment:
All 

Cause:
Wants to know if they can use a none B suffix version to replace the B suffix version.

Resolution:
The B suffix version was available to allow the customer to order the ATV312.....B  drive without the IO terminal and it would reduce cost if they are adding a communications module. 

If  you order the standard none B suffix version ATV312 you can remove the IO card and add the communications module in the field if needed.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.