{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is there an Assembly number that can be tied to the user map in the Tesys T LTMR product?

Issue:
Customer needs to tie the user map registers to an assembly number in order to reduce traffic on his network from explicit messaging.

Product Line:
LTMR Tesys T product.

Environment:
All models, All serial numbers.

Cause:
Unable to find supporting documentation.

Resolution:
There is no pre-defined instance in the Tesys-T that points to the user table.  Customer will need to either access this via explicit messaging or use instance 116 to pull all monitoring registers and then discard those that are not needed.

Schneider Electric Global

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: