Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
Osisense XU_Reliability data of the XUX1ARCNT16 photoelectric sensor MTTF, MTTFD
The reliability data of the XUX1ARCNT16 photoelectric sensor, single mode function (reflex system),are the following :
- MTTF = 592 years (mean time to failure),
- MTTFD = 1180 years (mean time to dangerous failure),
- DC = 0 (diagnostic coverage) of the sensor alone,
- mission time = 20 years.
They are used for the functional safety, according to the ISO 13849-1 standard (Performance Level). The MTTF calculation is made according to the IEC 62380 standard, value for 30°C temperature.
- MTTF = 592 years (mean time to failure),
- MTTFD = 1180 years (mean time to dangerous failure),
- DC = 0 (diagnostic coverage) of the sensor alone,
- mission time = 20 years.
They are used for the functional safety, according to the ISO 13849-1 standard (Performance Level). The MTTF calculation is made according to the IEC 62380 standard, value for 30°C temperature.
Did this answer your question?
Explore more
Explore more