Browse FAQs

Connecting the BMENOC03x1 to a Third party switch

Published date: 20 May 2020

Title
BMENOC03x1 connection to a Third party switch
 
Issue
Issue when connecting the BMENOC03x1 to a Third party switch
 
Product Line
BMENOC03x1 M580
 
Environment
Unity Pro
 
Resolution
 When connecting the BMENOC03x1 Ethernet module to a third-party switch, it may be necessary to turn Off the QoS service and Address Server service to be compatible with the third-party switch.
On the BMENOC03x1 module, the QoS service and the Address Server service are On by default.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.