Issue
To prevent the Trend server to run/start when the project is starting.
Product Line
PowerSCADA Expert 8.x
PowerSCADA Operations 9.0
note: applies to previous versions as well
Environment
Computer Setup Editor
INI file
Cause
In large systems with a lot of trend tags configured, it takes a long time for trend server to get to 'running' state. In cases were the project is being tested, it is not always necessary for the trends to run.