Browse FAQs

What is the heat dissipation value for the HMIG5U?

Published date: 29 May 2019

Issue:
What is the heat dissipation value for the HMIG5U?

Product Line:
HMIG5U, HMIG5U2

Resolution:

The caloric value of the product can be calculated with the following formula:

Calorific value=W[J/s]*[sec]=[J]

The power consumption values can be found in the user manual.

For example: According the OLH, the maximum power consumption (including the box module) of the HMIDT642 is 56 W.

After 100 seconds, the calorific value is:

Calorific value=56 W[J/s]*100 [sec]= 5600[J] 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.