Browse FAQs

Where to find documentation for the iEM3000 series meters?

Published date: 27 October 2019

Product Line
iEM3000 series

Cause
Would like further documentation on the iEM3000 series meters.

Resolution

See attached documents:

NEW! - Demand Readings added to meters with the following firmware versions or higher:

• iEM34x5 - V1.2.003 and higher
• iEM35x5 - V1.1.001 and higher
• iEM3465 and iEM3565 - BACnet V2.4 and higher

( iEM34xx and iEM35xx models with older firmware versions cannot be upgraded.)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.