{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do I break down an ATV660 part number to determine size, voltage, options, etc?
Issue:
ATV660 part number break down

Product Line:
Altivar 660 enclosed drives

Environment:
All

Cause:
Need to break down a part number

Resolution:
This information is located in the ATV660 Instruction Manual, which can be found here.

The options tables start in Section 2- Product Characteristics. Use the tables to go through the part number by each option.
The bulletin is also attached to this article.

Schneider Electric Global

Attachment(s)
ATV660 instruction bulletin.pdf [7.54 MB]