{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the weight capacity of NetShelter open frame racks: AR201, AR203A and AR204A?
Issue:
Static load rating is required.

Product Line:
NetShelter Open Frame Racks

Environment:
All models, all serial numbers.

Cause:
On the APC website, weight capacity is not noted in the Specifications tab of the product pages.

Resolution:
AR203A and AR204A Weight Capacity 2,000 lb (907.18 kg).
AR201 Weight Capacity 1,000 lb. (453.6 kg).

Schneider Electric Global