Browse FAQs

Which BMENOC03x1 module supports an email service?

Published date: 29 October 2019

Title
M580 and Email service
  
Issue
M580 and BMENOC0321 Email service
 
Product Line
BMENOC0321
 
Environment
Unity Pro
 
Resolution
 For the M580 PAC, the BMENOC0321 control network module includes an SMTP client. 
When the module receives a specific DATA_EXCH request over X Bus from the Unity Pro project, it sends an email message to the SMTP mail server. 
The Email notification service is setup in the Service configuration section of the BMENOC0321.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.