Browse FAQs

Does the BMXNOR0200 support an Email Client service?

Published date: 29 October 2019


Title
BMXNOR0200 Email Client service
 
Issue
BMXNOR0200 Web Designer Email client
 
Product Line
BMXNOR0200H
 
Environment
Unity Pro
 
Resolution
 Yes the BMXNOR0200 has a Email / SMS service and it is configured using Web Designer software.
NOTE: The SMS feature is supported only when a GSM or GPRS modem is configured. The SMS is sent only when the modem connection is not open.
 Please reference the user manual's Chapter 9 - How to Work with Email/SMS Service.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.