Browse FAQs

M580 BMENOC03x1 and RSTP

Published date: 29 October 2019


Title
M580 BMENOC03x1 and RSTP
 
Issue
M580 BMENOC03x1 and RSTP support
 
Product Line
M580 BMENOC0301 BMENOC0311
 
Environment
Unity Pro
 
Resolution
 The BMENOC03x1 Service Port (ETH1) does not run the Spanning Tree (STP/RSTP) protocol.
However , BMENOC03x1 Ethernet port 2 (ETH2) and port 3 (ETH3) do use the Spanning Tree (STP/RSTP) protocol.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.