{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
On an ATV630, why does the drive ramp all the way to low speed and high speed when my +/- speeds are pulsed?
Issue:
On an ATV630, the drive ramps all the way to low speed and high speed when my +/- speeds are pulsed.

Product Line:
Altivar Machines, Altivar Process Drives

Environment:
All models and serial numbers

Cause:
Drive ramps all the way up and down without stopping in between

Resolution:
This could be caused by any of the following:
  • The pulse isn't actually a pulse. Instead you're providing a sustained signal to the digital input
  • Acceleration time is too short. +/- speed ramping is based on acceleration speed
  • The pulse doesn't drop out long enough for the drive to recognize that it has dropped. Repeated input activation at too high speed can cause this
Try the following:
  • Make sure you're actually pulsing the inputs for activation
  • Try pulsing the inputs with a jumper wire from +24V to see if the behavior changes
  • Adjust acceleration time longer
  • Adjust deactivation of the digital inputs to a longer amount of time so the drive realizes the input has deactivated. The drive needs to see the signal drop in order to stop ramping

Schneider Electric Global